SPRUJB6B November 2024 – May 2025 AM2612 , AM2612-Q1
The PRU-ICSS UART0 peripheral can be placed in reduced-power modes to conserve power during periods of low activity. The power management of the PRU-ICSS UART0 peripheral and other PRU-ICSS peripherals is controlled by the device . The acts as a power management controller for all of the peripherals on the device. For more details on the power management procedures using the PSC, refer to the Power Management section.