Arguments: address and length
Effect: scratchpad = operand.
This command will cause an error if:
- Length is less than MAU_MIN_LENGTH
- Length is greater than MAU_MAX_LENGTH
- The memory address refers to a RAM or ROM slot, but those slots are not
configured
- The interval [address … address+length-1] does not all refer to the same type of
memory