SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
Lock/Commit feature allows the configured Enable bits for given errors to be locked to prevent further changes. To prevent changes, the Lock must be written, then the Commit. The Commit prevents the Lock from changing. Both Commit and Lock MMRs are reset by the warm reset (module reset) and by global soft reset.
When Lock is set to 1, the associated MMR values can not be changed. When Commit is set to 1, the Lock value can not be changed. Additionally, once set to 1, the Commit value can not be changed. Both Commit and Lock are reset by the warm reset (mod_g_rst_n) and by global soft reset.
All of the writeable MMRs have Commit/Lock bits except for the following: