SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
As an added security measure, the device boot ROM verifies the contents of the active CPU1 SECCFG sector using a CRC32 algorithm before loading the settings stored in the SECCFG sector into SSU registers. If the CRC check fails, the boot process is aborted. The SECCFG CRC is computed using the following parameters: