SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
eCAP modules can be synchronized with each other by selecting a common SYNCIN source. SYNCIN source for eCAP can be either software sync-in or external sync-in. The external sync-in signal can come from eCAP, X-Bar, or ePWM. The SWSYNC of the eCAP module is logical ORed with the SYNC signal as shown in Figure 25-7. The SYNC signal is defined by the selection of ECAPxSYNCINSEL[SEL] as shown in Figure 25-8.
The synchronization input source selection (ECAPSYNCINSEL) is the same as the ePWM Sync Input selection scheme. Please refer to the following table for the valid selection values table.
Figure 25-7 Details of the Counter and
Synchronization Block
Figure 25-8 eCAP
Synchronization Scheme