SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
The HRCAP enhancements leverage the existing eCAP interrupts (see Interrupt Control in the ECAP chapter) in addition to HRCALINT, which is used exclusively by the hardware calibration block. HRCALINT can be triggered by the following conditions:
Figure 29-2 shows this logic.
Figure 29-2 HRCAP Calibration