SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
FILE: spi_ex3_external_loopback.c
This program uses the external loopback between two SPI modules. Both the SPI FIFOs and interrupts are not used in this example. SPIA is configured as a peripheral and SPI B is configured as controller. This example demonstrates full duplex communication where both controller and peripheral transmits and receives data simultaneously.
External Connections
-GPIO16 and GPIO63 - SPIPICO -GPIO17 and GPIO25 - SPIPOCI -GPIO34 and GPIO26 - SPICLK -GPIO61 and GPIO27 - SPISTE
Watch Variables