SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
The digital filter works on a window of FIFO samples (SAMPWIN + 1) taken from the input. The filter output resolves to the majority value of the sample window, where majority is defined by the threshold (THRESH) value. If the majority threshold is not satisfied, the filter output remains unchanged.
For proper operation, the value of THRESH must be greater than SAMPWIN / 2.
A prescale function (CLKPRESCALE) determines the filter sampling rate, where the filter FIFO captures one sample every CLKPRESCALE system clocks. Old data from the FIFO is discarded.
A conceptual model of the digital filter is shown in Figure 32-12.
Figure 32-12 Digital Filter
Equivalent C code of the filter implementation is:
if (FILTER_OUTPUT == 0) {
if (Num_1s_in_SAMPWIN >= THRESH) {
FILTER_OUTPUT = 1;
}
}
else {
if (Num_0s_in_SAMPWIN >= THRESH) {
FILTER_OUTPUT = 0;
}
}
Filter Initialization Sequence
To make sure of proper operation of the digital filter, the following initialization sequence is recommended: