SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
FILE: led_ex2_blinky_cpu1_cpu2_cpu3_multi_c29x3.c
This example demonstrates how to configure LEDs using CPU1 and blink two LEDs using CPU2 (led_ex2_blinky_cpu1_cpu2_cpu3_multi_c29x2.c) and CPU3 (led_ex2_blinky_cpu1_cpu2_cpu3_multi_c29x3.c).
When using CCS for debugging this Multi-core example, after launching the debug session,
Note: Since CPU2 does not have FLASH access, the CPU2 application code is loaded to CPU1's FLASH, which is copied to CPU2 RAM by the CPU1 application. The CPU3 application code is loaded to its Flash (FRI-2) in FLASH BANKMODE2.
External Connections
Watch Variables