SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
The FSI receiver can continuously receive data and move the data from the receiver buffer with the RTDMA. A RTDMA trigger is generated every time a data frame has been received. This is concurrent with the FRAME_DONE signal that sets the RX_EVT_STS.FRAME_DONE flag. To receive continuous data with the RTDMA, some configurations need to be made on the receiver.
First, set RX_DMA_CTRL.DMA_EVT_EN to 1. This allows the RTDMA trigger to propagate to the RTDMA module. The receiver is now able to trigger a RTDMA event upon the reception of a data frame.
The RTDMA must also be configured properly for the FSI to receive the data. One way for using the receiver to continuously feed the RTDMA is:
Unlike the transmitter, there is no requirement to have the RTDMA channel that is handling the data buffer execute before the RTDMA channel handling the received tag and user data.