SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
The wait mode puts the CPU in a loop in the boot ROM code and does not branch to the user application code. The device can enter the wait boot mode either through manually being set or because of some issue during boot up. Using the wait boot mode is recommended when using a debugger to avoid any JTAG issues. There is an infinite for loop when entered in wait boot so user can easily halt CPU and load code when connected using debugger.
| Option | BOOTDEFx Value | Watchdog Status | Package Supported |
|---|---|---|---|
| 0 (default) | 0x04 | Disabled | All |
During boot ROM execution, there are situations where the CPU can enter a wait loop in the code. This state can occur for a variety of reasons.
Table 3-18 details the address ranges that the CPU PC register value reaches to if the CPU has entered one of these instances.
Following are the actions for entering wait boot mode:
| Program Counter Address Range | Description |
|---|---|
| 0x1535C | In Wait Boot mode |
| 0x14EB0 | In Wait Boot mode |