SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
The PWM Sync-chain on the MCU can be triggered either by the device external inputs from the GPIO using the input cross-bar or the PWM internal events when the chain is programmed appropriately. The SYNC0/1 inputs in this implementation also act as the external sync inputs to the PWM sync-chain. The integration is shown in Figure 31-18.
The additional select register added to the trigger crossbar register allows independent programming of the EXTSYNCx from either GPTRIP or SYNC0/1.
Figure 31-18 SYNC Integration for Control Functions - PWM SYNC