SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
FILE: adc_ex17_safety_checker.c
This example compares the absolute value of the two ADC conversion results with the set tolerance value.
The ADCA is used with A0 and A1 to compare the two ADC conversions. If the difference between two conversion results exceeds the value configured as tolerance then the ADC result safety checker tile generates an interrupt signal from out-of-tolerance.
External Connections
Watch Variables