SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
An asynchronous write is performed when any of the requesters mentioned in Section 13.2.2 request a write to memory in the asynchronous bank of EMIF. After the request is received, a write operation is initiated once the request becomes the EMIF's highest priority task, according to the priority scheme detailed in Section 13.2.13. In the event that the write request cannot be serviced by a single access cycle to the external device, multiple access cycles are performed by the EMIF until the entire request is fulfilled. The details of an asynchronous write operation in normal mode are described in Table 13-22. Also, Figure 13-12 shows an example timing diagram of a basic write operation.
| Time Interval | Pin Activity in Normal Mode | |
|---|---|---|
| Turnaround period | Once the write operation becomes the highest priority task for the EMIF, the EMIF waits for the programmed number of turn-around cycles before proceeding to the setup period of the operation. The number of wait cycles is taken directly from the TA field of the asynchronous n configuration register (ASYNC_CSn_CR). Between each access (write or read) EMIF inserts two cycles of delay even though TA field is programmed as 0. After the EMIF has waited for the turn-around cycles to complete, the EMIF again checks to make sure that the write operation is still the highest priority task. If so, the EMIF proceeds to the setup period of the operation. If the write operation is no longer the highest priority task, EMIF terminates the operation. | |
| Start of the setup period | The following actions occur at the start of the setup period:
| |
| Strobe period | The following actions occur at the start of the strobe period of a write operation:
| |
| End of the hold period | At the end of the hold period:
| |
Figure 13-12 Timing Waveform of an Asynchronous Write Cycle in Normal Mode