SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
FILE: uart_ex4_echoback.c
This test receives and echo-backs data through the UART A port.
A terminal such as 'putty' can be used to view the data from the UART and to send information to the UART. Characters received by the UART port are sent back to the host.
Running the Application Open a COM port with the following settings using a terminal:
The program will print out a greeting and then ask you to enter a character which it will echo back to the terminal.
Watch Variables
External Connections
Connect the UARTA port to a PC via a transceiver and cable.
Note: Avoid keeping the memory browser open while the execution is in progress.