SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
Step 3. MEP_ScaleFactor Initialization
The SFO() function does not require a starting scale factor value in MEP_ScaleFactor. Prior to using the MEP_ScaleFactor variable in application code, SFO() can be called to drive the MEP calibration module to calculate an MEP_ScaleFactor value.
As part of the one-time initialization code prior to using MEP_ScaleFactor, include the following: