SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
FILE: dcc_ex1_single_shot_verification.c
This program uses the Internal oscillator 2 as a reference clock to verify the frequency of the PLL.
The Dual-Clock Comparator Module 1 is used for the clock verification. The clocksource0 is the reference clock (Fclk0 = 10Mhz) and the clocksource1 is the clock that needs to be verified (Fclk1 = 200Mhz). Seed is the value that gets loaded into the Counter.
Please refer to the TRM for details on counter seed values to be set.
External Connections
Watch Variables