SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
Table 32-42 lists the memory-mapped registers for the FSI_RX_REGS registers. All register offset addresses not listed in Table 32-42 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Protection |
|---|---|---|---|
| 0h | RX_MAIN_CTRL | Receive main control register | |
| 8h | RX_OPER_CTRL | Receive operation control register | and LOCK |
| Ch | RX_FRAME_INFO | Receive frame control register | |
| Eh | RX_FRAME_TAG_UDATA | Receive frame tag and user data register | |
| 10h | RX_DMA_CTRL | Receive DMA event control register | and LOCK |
| 14h | RX_EVT_STS | Receive event and error status flag register | |
| 16h | RX_CRC_INFO | Receive CRC info of received and computed CRC | |
| 18h | RX_EVT_CLR | Receive event and error clear register | |
| 1Ah | RX_EVT_FRC | Receive event and error flag force register | |
| 1Ch | RX_BUF_PTR_LOAD | Receive buffer pointer load register | |
| 1Eh | RX_BUF_PTR_STS | Receive buffer pointer status register | |
| 20h | RX_FRAME_WD_CTRL | Receive frame watchdog control register | and LOCK |
| 24h | RX_FRAME_WD_REF | Receive frame watchdog counter reference | and LOCK |
| 28h | RX_FRAME_WD_CNT | Receive frame watchdog current count | |
| 2Ch | RX_PING_WD_CTRL | Receive ping watchdog control register | and LOCK |
| 2Eh | RX_PING_TAG | Receive ping tag register | |
| 30h | RX_PING_WD_REF | Receive ping watchdog counter reference | and LOCK |
| 34h | RX_PING_WD_CNT | Receive pingwatchdog current count | |
| 38h | RX_INT1_CTRL | Receive interrupt control register for RX_INT1 | and LOCK |
| 3Ah | RX_INT2_CTRL | Receive interrupt control register for RX_INT2 | and LOCK |
| 3Ch | RX_LOCK_CTRL | Receive lock control register | and LOCK |
| 40h | RX_ECC_DATA | Receive ECC data register | |
| 44h | RX_ECC_VAL | Receive ECC value register | |
| 48h | RX_ECC_SEC_DATA | Receive ECC corrected data register | |
| 4Ch | RX_ECC_LOG | Receive ECC log and status register | |
| 50h | RX_FRAME_TAG_CMP | Receive frame tag compare register | and LOCK |
| 52h | RX_PING_TAG_CMP | Receive ping tag compare register | and LOCK |
| 58h | RX_TRIG_CTRL_0 | Receive Trigger Control register 0 | and LOCK |
| 5Ch | RX_TRIG_WIDTH_0 | Receive Trigger Wdith register 0 | and LOCK |
| 60h | RX_DLYLINE_CTRL | Receive delay line control register | and LOCK |
| 64h | RX_TRIG_CTRL_1 | Receive Trigger Control register 1 | and LOCK |
| 68h | RX_TRIG_CTRL_2 | Receive Trigger Control register 2 | and LOCK |
| 6Ch | RX_TRIG_CTRL_3 | Receive Trigger Control register 3 | and LOCK |
| 70h | RX_VIS_1 | Receive debug visibility register 1 | |
| 74h | RX_UDATA_FILTER | Receive User Data Filter Control register | and LOCK |
| 80h + formula | RX_BUF_BASE_y | Base address for receive data buffer |
Complex bit access types are encoded to fit into small table cells. Table 32-43 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
RX_MAIN_CTRL is shown in Figure 32-37 and described in Table 32-44.
Return to the Summary Table.
Receive main control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| KEY | |||||||
| W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | DATA_FILTER_EN | INPUT_ISOLATE | SPI_PAIRING | INT_LOOPBACK | CORE_RST | ||
| R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | KEY | W | 0h | Write Key. In order to write to this register, 0xA5 must be written to this field at the same time. Otherwise, writes are ignored. The key is cleared immediately after writing, so it must be written again for every change to this register. Reset type: SYSRSn |
| 7-5 | RESERVED | R | 0h | Reserved |
| 4 | DATA_FILTER_EN | R/W | 0h | Data Filter Enable Bit. 0h (R/W) = Data filtering is disabled. 1h (R/W) = Data filtering is enabled. Reset type: SYSRSn |
| 3 | INPUT_ISOLATE | R/W | 0h | When set to 1, the FSI RX inputs (RXCLK, RXD0 and RXD1) will be isolated from what is driven from the device pins and will be held at inactive level of '1'.This isolation facilitates the user to switch the RX inputs to a different set of device pins and hence any potential glitch that could occur during the process of switching will not affect the RX module itself. Reset type: SYSRSn |
| 2 | SPI_PAIRING | R/W | 0h | Clock Pairing for SPI-like Behavior Enable bit This bit enables the internal clock pairing with the FSI TX module. This feature internally connects the TXCLK to RXCLK allowing the FSI TX module, acting as a SPI controller, to clock data into the receiver and out of the transmitter like a standard SPI module. This configuration is valid when the Module is in SPI mode only (RX_OPER_CTRL.SPI_MODE = 1) 0h (R/W) = SPI clock pairing is not enabled. 1h (R/W) = SPI clock pairing is enabled. The RXCLK will be internally connected to the TXCLK of the corresponding FSI module. Note: The KEY field must contatin 0xA5 for any write to this bit to take effect. Reset type: SYSRSn |
| 1 | INT_LOOPBACK | R/W | 0h | Internal Loopback Enable bit This bit enables the internal loopback functionality of the FSI receiver. By enabling this bit, a mux will select the signals coming directly from the corresponding FSI transmitter module rather than from the pins. 0h (R/W) = Internal loopback is disabled. The FSI RX module will receive signals coming from the pins. 1h (R/W) = Internal loopback is enabled. The FSI RX module will receive signals from the directly from FSI TX module rather than the pins. Note: The KEY field must contatin 0xA5 for any write to this bit to take effect. Reset type: SYSRSn |
| 0 | CORE_RST | R/W | 0h | Receiver Main Core Reset bit This bit controls the receiver main core reset. In order to receive any frame, this bit must be cleared. Note: For reset to take affect, the FSI RX module must be held in reset for at least 4 SYSCLK cycles. 0h (R/W) = Receiver core is not in reset and can receive frames. 1h (R/W) = Receiver core is held in reset. Note: The KEY field must contatin 0xA5 for any write to this bit to take effect. Reset type: SYSRSn |
RX_OPER_CTRL is shown in Figure 32-38 and described in Table 32-45.
Return to the Summary Table.
Receive operation control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | PING_WD_RST_MODE | ||||||
| R-0h | R/W-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ECC_SEL | N_WORDS | SPI_MODE | DATA_WIDTH | ||||
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-9 | RESERVED | R | 0h | Reserved |
| 8 | PING_WD_RST_MODE | R/W | 0h | Ping Watchdog Timeout Mode Select bit This bit selects the mode by which the ping watchdog counter is reset. The watchdog counter can be reset and restarted only by ping frames or by any received frame. 0h (R/W) = The ping watchdog counter will reset and restart only by ping frames. 1h (R/W) = The ping watchdog counter will reset and restart by any received frame. Reset type: SYSRSn |
| 7 | ECC_SEL | R/W | 0h | ECC Data Width Select bit This bit selects between whether the ECC computation is done on 16-bit or 32-bit words. 0h (R/W) = 32-bit ECC is used. 1h (R/W) = 16-bit ECC is used. Reset type: SYSRSn |
| 6-3 | N_WORDS | R/W | 0h | Number of Words to Receive This field defines the number of words which will be received in a DATA_N_WORD frame. This is a user-defined field that must match the corresponding field in the transmitter. Set this bitfield to be one less than the number of words to be received. This value is only applicable when the frame type received is DATA_N_WORD. 0h (R/W) = 1 data word frame (16-bit data). 1h (R/W) = 2 data word frame (32-bit data). .. Fh (R/W) = 16 data word frame (256-bit data). Reset type: SYSRSn |
| 2 | SPI_MODE | R/W | 0h | SPI Mode Enable bit This bit enables and disables the SPI compatibility mode of the FSI RX. The received data must be formatted as an FSI frame in order for the data to properly be received. SPI compatibility mode will allow FSI RX to receive data that is sent using SPI signal format. Refer to the applicable section in the FSI TRM chapter for more information. 0h (R/W) = FSI is in normal mode of operation. 1h (R/W) = FSI is operating in SPI compatibility mode. Reset type: SYSRSn |
| 1-0 | DATA_WIDTH | R/W | 0h | Receive Data Width Select bit These bits decide the number of data lines used for receiving data. 0h (R/W) = Data will be received on one data line, RXD0. 1h (R/W) = Data will be received on two data lines, RXD0 and RXD1. 2h, 3h (R/W) = Reserved Reset type: SYSRSn |
RX_FRAME_INFO is shown in Figure 32-39 and described in Table 32-46.
Return to the Summary Table.
Receive frame control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | FRAME_TYPE | ||||||
| R-0h | R-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-4 | RESERVED | R | 0h | Reserved |
| 3-0 | FRAME_TYPE | R | 0h | Received Frame Type This field indicates the type of non-ping frame that was successfully received last. Note: Ping frame reception does not update this field, we want to retain the last successful non-ping frame FRAME_TYPE and PING_FRAME_RCVD flag already conveys PING info to the user. 0100b (R/W) = A DATA_1_WORD frame was received (16-bit data). 0101b (R/W) = A DATA_2_WORD frame was received (32-bit data). 0110b (R/W) = A DATA_4_WORD frame was received (64-bit data). 0111b (R/W) = A DATA_6_WORD frame was received (96-bit data). 0011b (R/W) = A DATA_N_WORD frame was received. The N_WORD field will determine the number of words (1 to 16) to be sent. The number of words received must equal the value programmed in RX_OPER_CTRL.N_WORDS. 1111b (R/W) = An error frame was received. This frame can be used during error conditions or any condition where the transmitter wants to signal the receiver for attention. However, the user software is at liberty to use this for any purpose. 0001b, 0010b, and 1000b through 1110b are Reserved and should not be used. Reset type: SYSRSn |
RX_FRAME_TAG_UDATA is shown in Figure 32-40 and described in Table 32-47.
Return to the Summary Table.
Receive frame tag and user data register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| USER_DATA | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | FRAME_TAG | RESERVED | |||||
| R-0h | R-0h | R-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | USER_DATA | R | 0h | Received User Data This field contains the 8-bit user data field of the last successfully received frame. Reset type: SYSRSn |
| 7-5 | RESERVED | R | 0h | Reserved |
| 4-1 | FRAME_TAG | R | 0h | Received Frame Tag This field contains the 4-bit frame tag from the last successfully received frame. This is intentionally shifted into bits 4:1 so that the register can be used as a 32-bit address index based on the received tag. Reset type: SYSRSn |
| 0 | RESERVED | R | 0h | Reserved |
RX_DMA_CTRL is shown in Figure 32-41 and described in Table 32-48.
Return to the Summary Table.
Receive DMA event control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | DMA_EVT_EN | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-1 | RESERVED | R | 0h | Reserved |
| 0 | DMA_EVT_EN | R/W | 0h | DMA Event Enable bit This bit will enable a DMA Event to be generated upon the completion of a frame reception. 0h (R/W) = A DMA event will not be generated. 1h (R/W) = A DMA event will be generated upon the reception of a frame. Note: The DMA event will only be generated for data frames. Reset type: SYSRSn |
RX_EVT_STS is shown in Figure 32-42 and described in Table 32-49.
Return to the Summary Table.
Receive event and error status flag register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | ERROR_TAG_MATCH | DATA_TAG_MATCH | PING_TAG_MATCH | DATA_FRAME | FRAME_OVERRUN | PING_FRAME | ERR_FRAME |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BUF_UNDERRUN | FRAME_DONE | BUF_OVERRUN | EOF_ERR | TYPE_ERR | CRC_ERR | FRAME_WD_TO | PING_WD_TO |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15 | RESERVED | R | 0h | Reserved |
| 14 | ERROR_TAG_MATCH | R | 0h | Error Tag Match Flag This bit indicates that an error frame was received with a tag comparison matching the masked tag reference. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = No tag-matched error frame received. 1h (R) = A tag-matched error frame has been received. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 13 | DATA_TAG_MATCH | R | 0h | Data Tag Match Flag This bit indicates that a dataframe was received with a tag comparison matching the masked tag reference. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = No tag-matched data frame received. 1h (R) = A tag-matched data frame has been received. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 12 | PING_TAG_MATCH | R | 0h | Ping Tag Match Flag This bit indicates that a ping frame was received with a tag comparison matching the masked tag reference. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = No tag-matched ping frame received. 1h (R) = A tag-matched ping frame has been received. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 11 | DATA_FRAME | R | 0h | Data Frame Received Flag This bit indicates that an data frame has been received. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = No data frame has been received. 1h (R) = A data frame has been received. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 10 | FRAME_OVERRUN | R | 0h | Frame Overrun Flag This bit indicates that a frame overrun condition has occured. This bit gets set to 1 when a new DATA/ERROR frame is received and the corresponding DATA_FRAME_RCVD/ERROR_FRAME_RCVD flag is still set to 1. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = Frame overrun has not ocurred. 1h (R) = Frame overrun has ocurred. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 9 | PING_FRAME | R | 0h | Ping Frame Received Flag This bit indicates that an ping frame has been received. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = No ping frame has been received. 1h (R) = A ping frame has been received. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 8 | ERR_FRAME | R | 0h | Error Frame Received Flag This bit indicates that an error frame has been received. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = No error frame has been received. 1h (R) = An error frame has been received. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 7 | BUF_UNDERRUN | R | 0h | Receive Buffer Underrun Flag This bit indicates that a buffer underrun condition has occured in the receive buffer. This will happen when software reads the buffer which is empty and has no valid data. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = Receive Buffer Underrun has not ocurred. 1h (R) = Receive Buffer Underrun has ocurred. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 6 | FRAME_DONE | R | 0h | Frame Done Flag This bit indicates that a frame has been successfully received without error. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = No frame has been successfully received. 1h (R) = A frame has been successfully received. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 5 | BUF_OVERRUN | R | 0h | Receive Buffer Overrun Flag This bit indicates that a buffer overrun condition has occured in the receive buffer. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = Receive buffer overrun has not ocurred. 1h (R) = Receive buffer overrun has ocurred. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 4 | EOF_ERR | R | 0h | End-of-Frame Error Flag This bit indicates that an invalid end-of-frame bit pattern has been received. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = Invalid end-of-frame has not been received. 1h (R) = Invalid end-of-frame has been received To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 3 | TYPE_ERR | R | 0h | Frame Type Error Flag This bit inditcates that an invalid frame type has been received. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = Invalid frame type has not been received. 1h (R) = Invalid frame type has been received To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 2 | CRC_ERR | R | 0h | CRC Error Flag This bit indicates that a CRC error has occured. A CRC error will be generated on a data frame where the received CRC and the computed CRC do not match. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = CRC error has not occured. 1h (R) = CRC error has occured. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 1 | FRAME_WD_TO | R | 0h | Frame Watchdog Timeout Flag This bit indicates that the frame watchdog timer has timed out. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = Frame watchdog timeout has not occured. 1h (R) = Frame watchdog timeout has occured. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
| 0 | PING_WD_TO | R | 0h | Ping Watchdog Timeout Flag This bit indicates that the ping watchdog timer has timed out. Software can also force this bit to get set by writing to the RX_EVT_FRC register. 0h (R) = Ping watchdog timeout has not occured. 1h (R) = Ping watchdog timeout has occured. To clear this bit, write to the corresponding bit in the RX_EVT_CLR register. Reset type: SYSRSn |
RX_CRC_INFO is shown in Figure 32-43 and described in Table 32-50.
Return to the Summary Table.
Receive CRC info of received and computed CRC
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| CALC_CRC | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RX_CRC | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | CALC_CRC | R | 0h | Harware Calculated CRC Value This bitfield contains the CRC value that was calculated on the last received data. The contents of this bitfield are valid only when data frames are received. Note: The contents of this bitfield are invalid for ping and error frames. Reset type: SYSRSn |
| 7-0 | RX_CRC | R | 0h | Received CRC Value This bitfield contains the CRC value that was last received a frame. The contents of this bitfield are valid only when data frames are received. Note: The contents of this bitfield are invalid for ping and error frames. Reset type: SYSRSn |
RX_EVT_CLR is shown in Figure 32-44 and described in Table 32-51.
Return to the Summary Table.
Receive event and error clear register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | ERROR_TAG_MATCH | DATA_TAG_MATCH | PING_TAG_MATCH | DATA_FRAME | FRAME_OVERRUN | PING_FRAME | ERR_FRAME |
| R-0h | W-0h | W-0h | W-0h | W-0h | W-0h | W-0h | W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BUF_UNDERRUN | FRAME_DONE | BUF_OVERRUN | EOF_ERR | TYPE_ERR | CRC_ERR | FRAME_WD_TO | PING_WD_TO |
| W-0h | W-0h | W-0h | W-0h | W-0h | W-0h | W-0h | W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15 | RESERVED | R | 0h | Reserved |
| 14 | ERROR_TAG_MATCH | W | 0h | Error Tag Match Glag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 13 | DATA_TAG_MATCH | W | 0h | Data Tag Match Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 12 | PING_TAG_MATCH | W | 0h | Ping Tag Match Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 11 | DATA_FRAME | W | 0h | Data Frame Received Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 10 | FRAME_OVERRUN | W | 0h | Frame Overrun Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 9 | PING_FRAME | W | 0h | Ping Frame Received Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 8 | ERR_FRAME | W | 0h | Error Frame Received Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 7 | BUF_UNDERRUN | W | 0h | Receive Buffer Underrun Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (R/W) = Writing a 0 to this bit will have no effect. 1h (R/W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 6 | FRAME_DONE | W | 0h | Frame Done Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 5 | BUF_OVERRUN | W | 0h | Receive Buffer Overrun Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 4 | EOF_ERR | W | 0h | End-of-Frame Error Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 3 | TYPE_ERR | W | 0h | Frame Type Error Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 2 | CRC_ERR | W | 0h | CRC Error Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 1 | FRAME_WD_TO | W | 0h | Frame Watchdog Timeout Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
| 0 | PING_WD_TO | W | 0h | Ping Watchdog Timeout Flag Clear bit This bit clears the corresponding bit in the RX_EVT_STS register. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Writing a 1 to this bit will clear the corresponding bit in the RX_EVT_STS register to 0. Reset type: SYSRSn |
RX_EVT_FRC is shown in Figure 32-45 and described in Table 32-52.
Return to the Summary Table.
Receive event and error flag force register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | ERROR_TAG_MATCH | DATA_TAG_MATCH | PING_TAG_MATCH | DATA_FRAME | FRAME_OVERRUN | PING_FRAME | ERR_FRAME |
| R-0h | W-0h | W-0h | W-0h | W-0h | W-0h | W-0h | W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BUF_UNDERRUN | FRAME_DONE | BUF_OVERRUN | EOF_ERR | TYPE_ERR | CRC_ERR | FRAME_WD_TO | PING_WD_TO |
| W-0h | W-0h | W-0h | W-0h | W-0h | W-0h | W-0h | W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15 | RESERVED | R | 0h | Reserved |
| 14 | ERROR_TAG_MATCH | W | 0h | Error Tag Match Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 13 | DATA_TAG_MATCH | W | 0h | Data Tag Match Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 12 | PING_TAG_MATCH | W | 0h | Ping Tag Match Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 11 | DATA_FRAME | W | 0h | Data Frame Received Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 10 | FRAME_OVERRUN | W | 0h | Frame Overrun Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 9 | PING_FRAME | W | 0h | Ping Frame Received Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 8 | ERR_FRAME | W | 0h | Error Frame Received Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 7 | BUF_UNDERRUN | W | 0h | Receive Buffer Underrun Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 6 | FRAME_DONE | W | 0h | Frame Done Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 5 | BUF_OVERRUN | W | 0h | Receive Buffer Overrun Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 4 | EOF_ERR | W | 0h | End-of-Frame Error Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 3 | TYPE_ERR | W | 0h | Frame Type Error Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 2 | CRC_ERR | W | 0h | CRC Error Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 1 | FRAME_WD_TO | W | 0h | Frame Watchdog Timeout Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
| 0 | PING_WD_TO | W | 0h | Ping Watchdog Timeout Flag Force bit This bit will cause the corresponding bit in the RX_EVT_STS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR. 0h (W) = Writing a 0 to this bit will have no effect. 1h (W) = Force the corresponding bit in the RX_EVT_STS Register. Reset type: SYSRSn |
RX_BUF_PTR_LOAD is shown in Figure 32-46 and described in Table 32-53.
Return to the Summary Table.
Receive buffer pointer load register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | BUF_PTR_LOAD | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-4 | RESERVED | R | 0h | Reserved |
| 3-0 | BUF_PTR_LOAD | R/W | 0h | Buffer Pointer Load. This is the value to be loaded into the receive word pointer when written. This is to allow software to force the receiver to start storing the received data starting at a specific location in the buffer. NOTE: The value of the CURR_BUF_PTR in the RX_BUF_PTR_STS will not get reflected immediately. This will take effect only when there is a valid receive operation with incoming clocks after (3 RXCLK + 3 SYCLK) cycles. Reset type: SYSRSn |
RX_BUF_PTR_STS is shown in Figure 32-47 and described in Table 32-54.
Return to the Summary Table.
Receive buffer pointer status register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | CURR_WORD_CNT | ||||||
| R-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | CURR_BUF_PTR | ||||||
| R-0h | R-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-13 | RESERVED | R | 0h | Reserved |
| 12-8 | CURR_WORD_CNT | R | 0h | Words Available in the Receive Buffer This bitfield indicates the number of valid data words present in the receive buffer that have not been read by the application software. This bitfield is only valid when there is no active transfer. Note: This value will not be valid if there has been a buffer overrun or underrun condition. Reset type: SYSRSn |
| 7-4 | RESERVED | R | 0h | Reserved |
| 3-0 | CURR_BUF_PTR | R | 0h | Current Buffer Pointer Index This bitfield will show the current index of the buffer pointer. This value is only valid when there is no active transmission. Reset type: SYSRSn |
RX_FRAME_WD_CTRL is shown in Figure 32-48 and described in Table 32-55.
Return to the Summary Table.
Receive frame watchdog control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | FRAME_WD_EN | FRAME_WD_CNT_RST | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-2 | RESERVED | R | 0h | Reserved |
| 1 | FRAME_WD_EN | R/W | 0h | Frame Watchdog Counter Enable bit This bit will enable or disable the frame watchdog counter. The counter (RX_FRAME_WD_CNT) will begin counting from 0 when a valid start-of-frame pattern is received. When the reference value (RX_FRAME_WD_REF) is reached, it will generate a frame watchdog timeout event (RX_EVT_STS.FRAME_WD_TO) and the counter value will reset to 0 and continue counting on the next valid start-of-frame. 0h (R/W) = The frame watchdog counter is disabled and not running. 1h (R/W) = The frame watchdog counter logic is enabled and running. Reset type: SYSRSn |
| 0 | FRAME_WD_CNT_RST | R/W | 0h | Frame Watchdog Counter Reset bit This bit will reset the frame watchdog counter to 0. Writing a 1 to this bit will reset the frame watchdog counter to 0. The counter will stay in reset as long as this bit is set to 1. This bit needs to be cleared to 0 to use the counter 0h (R/W) = Clear the FRAME_WD_CNT_RST. 1h (W) = The frame watchdog counter will be reset to 0. Reset type: SYSRSn |
RX_FRAME_WD_REF is shown in Figure 32-49 and described in Table 32-56.
Return to the Summary Table.
Receive frame watchdog counter reference
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| FRAME_WD_REF | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | FRAME_WD_REF | R/W | 0h | Frame Watchdog Counter Reference Value This is the 32-bit reference value for the frame watchdog timeout counter. The counter will count up starting from 0 at a valid start-of-frame pattern and continue counting until this value is reached. Reset type: SYSRSn |
RX_FRAME_WD_CNT is shown in Figure 32-50 and described in Table 32-57.
Return to the Summary Table.
Receive frame watchdog current count
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| FRAME_WD_CNT | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | FRAME_WD_CNT | R | 0h | Frame Watchdog Counter Value This is the 32-bit read-only register which shows the current value of the frame watchdog counter. This counter is reset to 0 in a variety of ways: A write to FRME_WD_CNT_RST, a match with FRAME_WD_REF, or the reception of a successful data frame. Reset type: SYSRSn |
RX_PING_WD_CTRL is shown in Figure 32-51 and described in Table 32-58.
Return to the Summary Table.
Receive ping watchdog control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | PING_WD_EN | PING_WD_RST | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-2 | RESERVED | R | 0h | Reserved |
| 1 | PING_WD_EN | R/W | 0h | Ping Watchdog Counter Enable bit This bit will enable or disable the ping watchdog counter. The counter (RX_PING_WD_CNT) will begin counting from 0 when it is enabled. When the reference value (RX_PING_WD_REF) is reached, it will generate a ping watchdog timeout event (RX_EVT_STS.PING_WD_TO) and the counter value will reset to 0, and resume counting 0h (R/W) = The ping watchdog counter is disabled and not running. 1h (R/W) = The ping watchdog counter logic is enabled and running. Reset type: SYSRSn |
| 0 | PING_WD_RST | R/W | 0h | Ping Watchdog Counter Reset bit This bit will reset the ping watchdog counter to 0. Writing a 1 to this bit will reset the ping watchdog counter to 0. The counter will stay in reset as long as this bit is set to 1. This bit needs to be cleared to 0 to use the counter 0h (R/W) = Clear the PING_WD_RST. 1h (W) = The ping watchdog counter will be reset to 0. Reset type: SYSRSn |
RX_PING_TAG is shown in Figure 32-52 and described in Table 32-59.
Return to the Summary Table.
Receive ping tag register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | PING_TAG | RESERVED | |||||
| R-0h | R-0h | R-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-5 | RESERVED | R | 0h | Reserved |
| 4-1 | PING_TAG | R | 0h | Received Ping Frame Tag This field contains the 4-bit frame tag from the last successfully received ping frame. This is intentionally shifted into bits 4:1 so that the register can be used as a 32-bit address index based on the received tag. Reset type: SYSRSn |
| 0 | RESERVED | R | 0h | Reserved |
RX_PING_WD_REF is shown in Figure 32-53 and described in Table 32-60.
Return to the Summary Table.
Receive ping watchdog counter reference
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| PING_WD_REF | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | PING_WD_REF | R/W | 0h | Ping Watchdog Counter Reference Value This is the 32-bit reference value for the ping watchdog timeout counter. The counter will count up starting from 0 and continue counting until this value is reached. Reset type: SYSRSn |
RX_PING_WD_CNT is shown in Figure 32-54 and described in Table 32-61.
Return to the Summary Table.
Receive pingwatchdog current count
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| PING_WD_CNT | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | PING_WD_CNT | R | 0h | Ping Watchdog Counter Value This is the 32-bit read-only register which shows the current value of the ping watchdog counter. This counter is reset to 0 in a variety of ways: A write to PING_WD_RST, a match with PING_WD_REF, or the reception of a ping frame. Reset type: SYSRSn |
RX_INT1_CTRL is shown in Figure 32-55 and described in Table 32-62.
Return to the Summary Table.
Receive interrupt control register for RX_INT1
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | INT1_EN_ERROR_TAG_MATCH | INT1_EN_DATA_TAG_MATCH | INT1_EN_PING_TAG_MATCH | INT1_EN_DATA_FRAME | INT1_EN_FRAME_OVERRUN | INT1_EN_PING_FRAME | INT1_EN_ERR_FRAME |
| R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT1_EN_UNDERRUN | INT1_EN_FRAME_DONE | INT1_EN_OVERRUN | INT1_EN_EOF_ERR | INT1_EN_TYPE_ERR | INT1_EN_CRC_ERR | INT1_EN_FRAME_WD_TO | INT1_EN_PING_WD_TO |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15 | RESERVED | R | 0h | Reserved |
| 14 | INT1_EN_ERROR_TAG_MATCH | R/W | 0h | Enable Error Frame Received with Tag Match Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = An error frame received with matching tag will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 13 | INT1_EN_DATA_TAG_MATCH | R/W | 0h | Enable Data Frame Received with Tag Match Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A data frame received with matching tag will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 12 | INT1_EN_PING_TAG_MATCH | R/W | 0h | Enable Ping Frame Received with Tag Match Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A ping frame received with matching tag will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 11 | INT1_EN_DATA_FRAME | R/W | 0h | Enable Data Frame Received Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A data frame received event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 10 | INT1_EN_FRAME_OVERRUN | R/W | 0h | Enable Frame Overrun Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A frame overrun event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 9 | INT1_EN_PING_FRAME | R/W | 0h | Enable Ping Frame Received Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A ping frame received event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 8 | INT1_EN_ERR_FRAME | R/W | 0h | Enable ERROR Frame Received Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A error frame received event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 7 | INT1_EN_UNDERRUN | R/W | 0h | Enable Buffer Underrun Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A buffer underrun event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 6 | INT1_EN_FRAME_DONE | R/W | 0h | Enable Frame Done Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A frame done event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 5 | INT1_EN_OVERRUN | R/W | 0h | Enable Receive Buffer Overrun Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A receive buffer overrun event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 4 | INT1_EN_EOF_ERR | R/W | 0h | Enable End-of-Frame Error Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = An end-of-frame error event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 3 | INT1_EN_TYPE_ERR | R/W | 0h | Enable Frame Type Error Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A frame type error event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 2 | INT1_EN_CRC_ERR | R/W | 0h | Enable CRC Error Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A CRC error will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 1 | INT1_EN_FRAME_WD_TO | R/W | 0h | Enable Frame Watchdog Timeout Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A frame watchdog timeout event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 0 | INT1_EN_PING_WD_TO | R/W | 0h | Enable Ping Watchdog Timeout Interrupt to INT1 bit This is an enable register which decides whether an interrupt (RX_INT1) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT1. 1h (R/W) = A ping watchdog timeout event will trigger an interrupt on RX_INT1. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
RX_INT2_CTRL is shown in Figure 32-56 and described in Table 32-63.
Return to the Summary Table.
Receive interrupt control register for RX_INT2
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | INT2_EN_ERROR_TAG_MATCH | INT2_EN_DATA_TAG_MATCH | INT2_EN_PING_TAG_MATCH | INT2_EN_DATA_FRAME | INT2_EN_FRAME_OVERRUN | INT2_EN_PING_FRAME | INT2_EN_ERR_FRAME |
| R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INT2_EN_UNDERRUN | INT2_EN_FRAME_DONE | INT2_EN_OVERRUN | INT2_EN_EOF_ERR | INT2_EN_TYPE_ERR | INT2_EN_CRC_ERR | INT2_EN_FRAME_WD_TO | INT2_EN_PING_WD_TO |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15 | RESERVED | R | 0h | Reserved |
| 14 | INT2_EN_ERROR_TAG_MATCH | R/W | 0h | Enable Error Frame Received with Tag Match Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = An error frame received with matching tag will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 13 | INT2_EN_DATA_TAG_MATCH | R/W | 0h | Enable Data Frame Received with Tag Match Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A data frame received with matching tag will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 12 | INT2_EN_PING_TAG_MATCH | R/W | 0h | Enable Ping Frame Received with Tag Match Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A ping frame received with matching tag will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 11 | INT2_EN_DATA_FRAME | R/W | 0h | Enable Data Frame Received Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A data frame received event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 10 | INT2_EN_FRAME_OVERRUN | R/W | 0h | Enable Frame Overrun Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A frame overrun event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 9 | INT2_EN_PING_FRAME | R/W | 0h | Enable Ping Frame Received Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A ping frame received event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 8 | INT2_EN_ERR_FRAME | R/W | 0h | Enable Error Frame Received Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A error frame received event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 7 | INT2_EN_UNDERRUN | R/W | 0h | Enable Buffer Underrun Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A buffer underrun event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 6 | INT2_EN_FRAME_DONE | R/W | 0h | Enable Frame Done Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A frame done event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 5 | INT2_EN_OVERRUN | R/W | 0h | Enable Buffer Overrun Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A buffer overrun event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 4 | INT2_EN_EOF_ERR | R/W | 0h | Enable End-of-Frame Error Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = An end-of-frame error event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 3 | INT2_EN_TYPE_ERR | R/W | 0h | Enable Frame Type Error Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A frame type error event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 2 | INT2_EN_CRC_ERR | R/W | 0h | Enable CRC Error Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A CRC error will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 1 | INT2_EN_FRAME_WD_TO | R/W | 0h | Enable Frame Watchdog Timeout Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A frame watchdog timeout event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
| 0 | INT2_EN_PING_WD_TO | R/W | 0h | Enable Ping Watchdog Timeout Interrupt to INT2 bit This is an enable register which decides whether an interrupt (RX_INT2) will be generated on the enabled event. 0h (R/W) = This event will not trigger an interrupt on RX_INT2. 1h (R/W) = A ping watchdog timeout event will trigger an interrupt on RX_INT2. The event itself will be latched in the corresponding bit in the RX_EVT_STS Register Reset type: SYSRSn |
RX_LOCK_CTRL is shown in Figure 32-57 and described in Table 32-64.
Return to the Summary Table.
Receive lock control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| KEY | |||||||
| W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | LOCK | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | KEY | W | 0h | Write Key. In order to write to this register, 0xA5 must be written to this field at the same time. Otherwise, writes are ignored. The key is cleared immediately after writing, so it must be written again for every change to this register. Reset type: SYSRSn |
| 7-1 | RESERVED | R | 0h | Reserved |
| 0 | LOCK | R/W | 0h | Control Register Lock Enable bit This bit locks the contents of all the receive control registers that support a lock protection. Once locked, further writes will not take effect until SYSRS unlocks the register. Once set, further writes even to this bit will be ignored. 0h (R/W) = Receive control registers can be modified and are not locked. 1h (R/W) = Receive control registers are locked and cannot be modified until this bit is cleared by SYSRS. Any further writes to this bit are ignored. Note: The KEY field must contatin 0xA5 for any write to this bit to take effect. Reset type: SYSRSn |
RX_ECC_DATA is shown in Figure 32-58 and described in Table 32-65.
Return to the Summary Table.
Receive ECC data register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DATA_HIGH | DATA_LOW | ||||||||||||||||||||||||||||||
| R/W-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | DATA_HIGH | R/W | 0h | Upper 16 bits of ECC Data Writing to this bitfield will cause the ECC logic to compute the ECC(SEC-DED) the entire 32-bit register and update TX_ECC_VAL register with the results. Software should write to these 16 bits of the register in a 32-bit write when needing to compute ECC for 32-bits for the full TX_ECC_DATA register. Reset type: SYSRSn |
| 15-0 | DATA_LOW | R/W | 0h | Lower 16 bits of ECC Data Writing to this bitfield will cause the ECC logic to compute the ECC(SEC-DED) for these 16 bits and update the TX_ECC_VAL register with the results. Software should write to these register bits as a 16-bit write when needing to compute ECC for 16-bits. Reset type: SYSRSn |
RX_ECC_VAL is shown in Figure 32-59 and described in Table 32-66.
Return to the Summary Table.
Receive ECC value register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ECC_VAL | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-7 | RESERVED | R | 0h | Reserved |
| 6-0 | ECC_VAL | R/W | 0h | ECC Value for SEC-DED check This field contains the ECC value to be used for SEC-DED either for 16-bit or 32-bit data in the RX_ECC_DATA register. Reset type: SYSRSn |
RX_ECC_SEC_DATA is shown in Figure 32-60 and described in Table 32-67.
Return to the Summary Table.
Receive ECC corrected data register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SEC_DATA | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | SEC_DATA | R | 0h | ECC Single Error Corrected Data The ECC corrected data will be available in this register. This value is valid only when there are no bit errors, or a single bit error was detected. Otherwise, the contents of this register are invalid and should not be used. Reset type: SYSRSn |
RX_ECC_LOG is shown in Figure 32-61 and described in Table 32-68.
Return to the Summary Table.
Receive ECC log and status register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | MBE | SBE | |||||
| R-0h | R-1h | R-1h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-2 | RESERVED | R | 0h | Reserved |
| 1 | MBE | R | 1h | Multiple Bit Errors Detected This bit indicates the occurrence of multiple bit errors.The data is corrupted and cannot be corrected. If this bit is set, the data present in RX_ECC_SEC_DATA is invalid and should not be used. 0h (R) Multiple Bit Errors were not detected. Check the SBE bit for single bit errors. 1h (R) Multiple Bit Errors were detected. The data is not able to be corrected. The value present in RX_ECC_SEC_DATA is invalid and should not be used. Reset type: SYSRSn |
| 0 | SBE | R | 1h | Single Bit Error Detected This bit indicates the occurrence of a single bit error in the data. The data is autocorrected and placed into the RX_ECC_SEC_DATA register. This bit is valid only if MBE is 0. 0h (R) No bit errors were detected. The value in RX_ECC_SEC_DATA is correct. 1h (R) A single bit error was detected and corrected. The corrected data is present in RX_ECC_SEC_DATA. Reset type: SYSRSn |
RX_FRAME_TAG_CMP is shown in Figure 32-62 and described in Table 32-69.
Return to the Summary Table.
Receive frame tag compare register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | BROADCAST_EN | CMP_EN | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| TAG_MASK | TAG_REF | ||||||
| R/W-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-10 | RESERVED | R | 0h | Reserved |
| 9 | BROADCAST_EN | R/W | 0h | Broadcast Enable bit This will enable the reception of a ping frame broadcast. When this bit is set, bit 3 of the received tag will be treated as a broadcast notification. If bit 3 of the received tag is set to 1, a ping tag match event will be triggered regardless of the. A match caused by the comparison of TAG_MASK and TAG_REF will still be considered a match and the frame tag match event will be triggered as normal This bit only takes effect only if CMP_EN is set to 1. 0h (R/W) Broadcast frame match disabled. 1h (R/W) Broadcast frame match enabled. Reset type: SYSRSn |
| 8 | CMP_EN | R/W | 0h | Frame Tag Compare Enable bit Set this bit to enable the comparison of an incoming frame tag and the value stored in the frame tag reference. A match caused by the comparison of TAG_MASK, TAG_REF, and the incoming frame tag will trigger the apprpriate frame tag match event. 0h (R/W) Frame tag comparison is disabled. 1h (R/W) Frame tag comparison is enabled. Reset type: SYSRSn |
| 7-4 | TAG_MASK | R/W | 0h | Frame Tag Mask Any bit position in this register set to 0 will be used in the comparison of the incoming frame tag and the value stored in TAG_REF. A bit position set to 1 will be ignored in the tag comparison. This mask value is used only for non-ping frames. Reset type: SYSRSn |
| 3-0 | TAG_REF | R/W | 0h | Frame Tag Reference The reference tag to check against when comparing the TAG_MASK and the incoming frame tag. This reference value is used only for non-ping frames. Reset type: SYSRSn |
RX_PING_TAG_CMP is shown in Figure 32-63 and described in Table 32-70.
Return to the Summary Table.
Receive ping tag compare register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | BROADCAST_EN | CMP_EN | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| TAG_MASK | TAG_REF | ||||||
| R/W-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-10 | RESERVED | R | 0h | Reserved |
| 9 | BROADCAST_EN | R/W | 0h | Broadcast Enable bit This will enable the reception of a ping frame broadcast. When this bit is set, bit 3 of the received tag will be treated as a broadcast notification. If bit 3 of the received tag is set to 1, a ping tag match event will be triggered regardless of the. A match caused by the comparison of TAG_MASK and TAG_REF will still be considered a match and the ping tag match event will be triggered as normal This bit only takes effect only if CMP_EN is set to 1. 0h (R/W) Broadcast frame match disabled. 1h (R/W) Broadcast frame match enabled. Reset type: SYSRSn |
| 8 | CMP_EN | R/W | 0h | Ping Tag Compare Enable bit Set this bit to enable the comparison of an incoming ping tag and the value stored in the ping tag reference. A match caused by the comparison of TAG_MASK, TAG_REF, and the incoming ping tag will trigger a ping frame tag match event. 0h (R/W) Ping tag comparison is disabled. 1h (R/W) Ping tag comparison is enabled. Reset type: SYSRSn |
| 7-4 | TAG_MASK | R/W | 0h | Ping Tag Mask Any bit position in this register set to 0 will be used in the comparison of the incoming ping frame tag and the value stored in TAG_REF. A bit position set to 1 will be ignored in the tag comparison. This mask value is used only for ping frames. Reset type: SYSRSn |
| 3-0 | TAG_REF | R/W | 0h | Ping Tag Reference The reference tag to check against when comparing the TAG_MASK and the incoming ping tag. This reference value is used only for ping frames. Reset type: SYSRSn |
RX_TRIG_CTRL_0 is shown in Figure 32-64 and described in Table 32-71.
Return to the Summary Table.
Receive Trigger Control register 0
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TRIG_SEL | TRIG_EN | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RX_TRIG_DLY | R/W | 0h | This is the 24 bit count of the trigger delay in SYSCLK cycles. If enabled, the Trigger-1 output of the trigger module will generate a 3 SYSCLK wide trigger pulse after the selected input trigger source sees a rising edge with a delay defined by this 24-bt value. Reset type: SYSRSn |
| 7-5 | RESERVED | R | 0h | Reserved |
| 4-1 | TRIG_SEL | R/W | 0h | This is the mux select value which selects which of the inputs will be used as the trigger source. Reset type: SYSRSn |
| 0 | TRIG_EN | R/W | 0h | This is the enable for the RX output trigger generation. The output triggers will be generated only if this bit is set to 1. If this bit is 0, then no trigger will be generated by this module. Reset type: SYSRSn |
RX_TRIG_WIDTH_0 is shown in Figure 32-65 and described in Table 32-72.
Return to the Summary Table.
Receive Trigger Wdith register 0
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RX_TRIG_WIDTH | ||||||||||||||||||||||||||||||
| R-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | RX_TRIG_WIDTH | R/W | 0h | This register decides the width(in SYSCLK cycles) of wide pulse output of the RX trigger module. Reset type: SYSRSn |
RX_DLYLINE_CTRL is shown in Figure 32-66 and described in Table 32-73.
Return to the Summary Table.
Receive delay line control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | RXD1_DLY | RXD0_DLY | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RXD0_DLY | RXCLK_DLY | ||||||
| R/W-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15 | RESERVED | R | 0h | Reserved |
| 14-10 | RXD1_DLY | R/W | 0h | Delay Line Tap Select for RXD1 This bitfield selects the number of delay elements inserted into the RXD1 path from the pin boundary to the receiver core. 0h (R/W) Zero delay elements are included in the RXD1 path. RXD1 is taken directly from the pin. 1h (R/W) One delay element is included in the RXD1 path. 2h (R/W) Two delay elements are included in the RXD1 path. ... 1Fh (R/W) 31 delay elements are included in the RXD1 path, the maximum. Reset type: SYSRSn |
| 9-5 | RXD0_DLY | R/W | 0h | Delay Line Tap Select for RXD0 This bitfield selects the number of delay elements inserted into the RXD0 path from the pin boundary to the receiver core. 0h (R/W) Zero delay elements are included in the RXD0 path. RXD0 is taken directly from the pin. 1h (R/W) One delay element is included in the RXD0 path. 2h (R/W) Two delay elements are included in the RXD0 path. ... 1Fh (R/W) 31 delay elements are included in the RXD0 path, the maximum. Reset type: SYSRSn |
| 4-0 | RXCLK_DLY | R/W | 0h | Delay Line Tap Select for RXCLK This bitfield selects the number of delay elements inserted into the RXCLK path from the pin boundary to the receiver core. 0h (R/W) Zero delay elements are included in the RXCLK path. RXCLK is taken directly from the pin. 1h (R/W) One delay element is included in the RXCLK path. 2h (R/W) Two delay elements are included in the RXCLK path. ... 1Fh (R/W) 31 delay elements are included in the RXCLK path, the maximum. Reset type: SYSRSn |
RX_TRIG_CTRL_1 is shown in Figure 32-67 and described in Table 32-74.
Return to the Summary Table.
Receive Trigger Control register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TRIG_SEL | TRIG_EN | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RX_TRIG_DLY | R/W | 0h | This is the 24 bit count of the trigger delay in SYSCLK cycles. If enabled, the Trigger-1 output of the trigger module will generate a 3 SYSCLK wide trigger pulse after the selected input trigger source sees a rising edge with a delay defined by this 24-bt value. Reset type: SYSRSn |
| 7-5 | RESERVED | R | 0h | Reserved |
| 4-1 | TRIG_SEL | R/W | 0h | This is the mux select value which selects which of the inputs will be used as the trigger source. Reset type: SYSRSn |
| 0 | TRIG_EN | R/W | 0h | This is the enable for the RX output trigger generation. The output triggers will be generated only if this bit is set to 1. If this bit is 0, then no trigger will be generated by this module. Reset type: SYSRSn |
RX_TRIG_CTRL_2 is shown in Figure 32-68 and described in Table 32-75.
Return to the Summary Table.
Receive Trigger Control register 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TRIG_SEL | TRIG_EN | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RX_TRIG_DLY | R/W | 0h | This is the 24 bit count of the trigger delay in SYSCLK cycles. If enabled, the Trigger-1 output of the trigger module will generate a 3 SYSCLK wide trigger pulse after the selected input trigger source sees a rising edge with a delay defined by this 24-bt value. Reset type: SYSRSn |
| 7-5 | RESERVED | R | 0h | Reserved |
| 4-1 | TRIG_SEL | R/W | 0h | This is the mux select value which selects which of the inputs will be used as the trigger source. Reset type: SYSRSn |
| 0 | TRIG_EN | R/W | 0h | This is the enable for the RX output trigger generation. The output triggers will be generated only if this bit is set to 1. If this bit is 0, then no trigger will be generated by this module. Reset type: SYSRSn |
RX_TRIG_CTRL_3 is shown in Figure 32-69 and described in Table 32-76.
Return to the Summary Table.
Receive Trigger Control register 3
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RX_TRIG_DLY | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TRIG_SEL | TRIG_EN | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RX_TRIG_DLY | R/W | 0h | This is the 24 bit count of the trigger delay in SYSCLK cycles. If enabled, the Trigger-1 output of the trigger module will generate a 3 SYSCLK wide trigger pulse after the selected input trigger source sees a rising edge with a delay defined by this 24-bt value. Reset type: SYSRSn |
| 7-5 | RESERVED | R | 0h | Reserved |
| 4-1 | TRIG_SEL | R/W | 0h | This is the mux select value which selects which of the inputs will be used as the trigger source. Reset type: SYSRSn |
| 0 | TRIG_EN | R/W | 0h | This is the enable for the RX output trigger generation. The output triggers will be generated only if this bit is set to 1. If this bit is 0, then no trigger will be generated by this module. Reset type: SYSRSn |
RX_VIS_1 is shown in Figure 32-70 and described in Table 32-77.
Return to the Summary Table.
Receive debug visibility register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RX_CORE_STS | RESERVED | |||||
| R-0h | R-0h | R-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3 | RX_CORE_STS | R | 0h | Receiver Core Status bit This bit indicates the status of the receiver core. If this bit is set, the receiver should undergo a reset and subsequent resynchronization with the transmitter. This bit will be always be set when the receiver has detected and end of frame error or a frame type error. This bit can also be set if the receiver becomes corrupted due to noise on the signal lines. If the receiver has experienced a ping watchdog or frame watchdog timeout, this bit should be read to determine if the cause was due to a corrupt transaction, thus putting the receiver core into an unrecoverable state. Only a soft reset will reset the recevier core and thus reset this bit. 0h (R) The receiver core is operating normally. 1h (R) The receiver core has entered into an error state and should be reset. Reset type: SYSRSn |
| 2-0 | RESERVED | R | 0h | Reserved |
RX_UDATA_FILTER is shown in Figure 32-71 and described in Table 32-78.
Return to the Summary Table.
Receive User Data Filter Control register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| UDATA_MASK | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| UDATA_REF | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-8 | UDATA_MASK | R/W | 0h | Bit Mask to be used for comparing the USERDATA field when filtering is enabled. Every bit that is '1' in this register will be masked for comparison. If a bit position is '1', then it will be considered a successful match for that bit position. Reset type: SYSRSn |
| 7-0 | UDATA_REF | R/W | 0h | Reference to be used for comparing the USERDATA field when filtering is enabled. Reset type: SYSRSn |
RX_BUF_BASE_y is shown in Figure 32-72 and described in Table 32-79.
Return to the Summary Table.
Base address for receive data buffer
Offset = 80h + (y * 2h); where y = 0h to Fh
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| BASE_ADDRESS | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BASE_ADDRESS | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-0 | BASE_ADDRESS | R | 0h | Receive Data Buffer Base Address This is the base address of the 16-word data buffer used by the receiver. Reset type: SYSRSn |