SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
The SCI receiver is enabled to receive messages, if both the RX FUNC bit and the RXENA bit are set to 1. If the RX FUNC bit is not set, the LINRX pin functions as a general-purpose I/O pin rather than as an SCI function pin.
SCI module can receive data in one of the following modes:
After a valid idle period is detected, data is automatically received as the data arrives on the LINRX pin.