SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1
Table 19-71 lists the memory-mapped registers for the ICL_XBAR_REGS registers. All register offset addresses not listed in Table 19-71 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Protection |
|---|---|---|---|
| 30h | ICLXBAROutInvert | Output Signal Invert Select | |
| 80h | ICLXBARLock | Configuration Lock register | |
| 100h + formula | ICLXBARG0SEL_j | ICLXBAR G0 Input Select | |
| 104h + formula | ICLXBARG1SEL_j | ICLXBAR G1 Input Select | |
| 108h + formula | ICLXBARG2SEL_j | ICLXBAR G2 Input Select |
Complex bit access types are encoded to fit into small table cells. Table 19-72 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| Write Type | ||
| W | W | Write |
| WSonce | W Sonce | Write Set once |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
ICLXBAROutInvert is shown in Figure 19-54 and described in Table 19-73.
Return to the Summary Table.
Output Signal Invert Select
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| XBAR16 | XBAR15 | XBAR14 | XBAR13 | XBAR12 | XBAR11 | XBAR10 | XBAR9 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| XBAR8 | XBAR7 | XBAR6 | XBAR5 | XBAR4 | XBAR3 | XBAR2 | XBAR1 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R-0 | 0h | Reserved |
| 15 | XBAR16 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 14 | XBAR15 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 13 | XBAR14 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 12 | XBAR13 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 11 | XBAR12 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 10 | XBAR11 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 9 | XBAR10 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 8 | XBAR9 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 7 | XBAR8 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 6 | XBAR7 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 5 | XBAR6 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 4 | XBAR5 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 3 | XBAR4 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 2 | XBAR3 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 1 | XBAR2 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
| 0 | XBAR1 | R/W | 0h | Select Output: 0 No inversion 1 Output inverted Reset type: XRSn |
ICLXBARLock is shown in Figure 19-55 and described in Table 19-74.
Return to the Summary Table.
Configuration Lock register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| KEY | |||||||
| R-0/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| KEY | |||||||
| R-0/W-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | LOCK | ||||||
| R-0-0h | R/WSonce-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | KEY | R-0/W | 0h | Bit-0 of this register can be set only if KEY= 0x5a5a Reset type: XRSn |
| 15-1 | RESERVED | R-0 | 0h | Reserved |
| 0 | LOCK | R/WSonce | 0h | Locks the configuration for EICL-XBAR. Once the configuration is locked, writes to the below registers for EICL-XBAR is blocked. Registers Affected by the LOCK mechanism: ICLXBAR Gx SEL ICLXBAR.Invert 0: Writes to the above registers are allowed 1: Writes to the above registers are blocked Note: [1] LOCK mechanism only apples to writes. Reads are never blocked. Reset type: XRSn |
ICLXBARG0SEL_j is shown in Figure 19-56 and described in Table 19-75.
Return to the Summary Table.
ICLXBAR G0 Input Select
Offset = 100h + (j * 40h); where j = 0h to Fh
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| INPUT31 | INPUT30 | INPUT29 | INPUT28 | INPUT27 | INPUT26 | INPUT25 | INPUT24 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| INPUT23 | INPUT22 | INPUT21 | INPUT20 | INPUT19 | INPUT18 | INPUT17 | INPUT16 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| INPUT15 | INPUT14 | INPUT13 | INPUT12 | INPUT11 | INPUT10 | INPUT9 | INPUT8 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INPUT7 | INPUT6 | INPUT5 | INPUT4 | INPUT3 | INPUT2 | INPUT1 | INPUT0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | INPUT31 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 30 | INPUT30 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 29 | INPUT29 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 28 | INPUT28 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 27 | INPUT27 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 26 | INPUT26 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 25 | INPUT25 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 24 | INPUT24 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 23 | INPUT23 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 22 | INPUT22 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 21 | INPUT21 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 20 | INPUT20 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 19 | INPUT19 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 18 | INPUT18 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 17 | INPUT17 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 16 | INPUT16 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 15 | INPUT15 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 14 | INPUT14 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 13 | INPUT13 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 12 | INPUT12 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 11 | INPUT11 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 10 | INPUT10 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 9 | INPUT9 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 8 | INPUT8 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 7 | INPUT7 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 6 | INPUT6 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 5 | INPUT5 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 4 | INPUT4 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 3 | INPUT3 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 2 | INPUT2 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 1 | INPUT1 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 0 | INPUT0 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
ICLXBARG1SEL_j is shown in Figure 19-57 and described in Table 19-76.
Return to the Summary Table.
ICLXBAR G1 Input Select
Offset = 104h + (j * 40h); where j = 0h to Fh
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| INPUT31 | INPUT30 | INPUT29 | INPUT28 | INPUT27 | INPUT26 | INPUT25 | INPUT24 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| INPUT23 | INPUT22 | INPUT21 | INPUT20 | INPUT19 | INPUT18 | INPUT17 | INPUT16 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| INPUT15 | INPUT14 | INPUT13 | INPUT12 | INPUT11 | INPUT10 | INPUT9 | INPUT8 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INPUT7 | INPUT6 | INPUT5 | INPUT4 | INPUT3 | INPUT2 | INPUT1 | INPUT0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | INPUT31 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 30 | INPUT30 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 29 | INPUT29 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 28 | INPUT28 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 27 | INPUT27 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 26 | INPUT26 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 25 | INPUT25 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 24 | INPUT24 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 23 | INPUT23 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 22 | INPUT22 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 21 | INPUT21 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 20 | INPUT20 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 19 | INPUT19 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 18 | INPUT18 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 17 | INPUT17 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 16 | INPUT16 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 15 | INPUT15 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 14 | INPUT14 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 13 | INPUT13 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 12 | INPUT12 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 11 | INPUT11 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 10 | INPUT10 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 9 | INPUT9 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 8 | INPUT8 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 7 | INPUT7 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 6 | INPUT6 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 5 | INPUT5 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 4 | INPUT4 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 3 | INPUT3 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 2 | INPUT2 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 1 | INPUT1 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 0 | INPUT0 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
ICLXBARG2SEL_j is shown in Figure 19-58 and described in Table 19-77.
Return to the Summary Table.
ICLXBAR G2 Input Select
Offset = 108h + (j * 40h); where j = 0h to Fh
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| INPUT31 | INPUT30 | INPUT29 | INPUT28 | INPUT27 | INPUT26 | INPUT25 | INPUT24 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| INPUT23 | INPUT22 | INPUT21 | INPUT20 | INPUT19 | INPUT18 | INPUT17 | INPUT16 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| INPUT15 | INPUT14 | INPUT13 | INPUT12 | INPUT11 | INPUT10 | INPUT9 | INPUT8 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INPUT7 | INPUT6 | INPUT5 | INPUT4 | INPUT3 | INPUT2 | INPUT1 | INPUT0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | INPUT31 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 30 | INPUT30 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 29 | INPUT29 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 28 | INPUT28 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 27 | INPUT27 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 26 | INPUT26 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 25 | INPUT25 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 24 | INPUT24 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 23 | INPUT23 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 22 | INPUT22 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 21 | INPUT21 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 20 | INPUT20 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 19 | INPUT19 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 18 | INPUT18 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 17 | INPUT17 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 16 | INPUT16 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 15 | INPUT15 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 14 | INPUT14 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 13 | INPUT13 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 12 | INPUT12 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 11 | INPUT11 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 10 | INPUT10 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 9 | INPUT9 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 8 | INPUT8 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 7 | INPUT7 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 6 | INPUT6 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 5 | INPUT5 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 4 | INPUT4 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 3 | INPUT3 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 2 | INPUT2 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 1 | INPUT1 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |
| 0 | INPUT0 | R/W | 0h | Select input: 0 Not Selected 1 Input Selected Reset type: XRSn |