SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
An asynchronous read is performed when any of the requesters mentioned in Section 13.2.2 request a read from the attached asynchronous memory. After the request is received, a read operation is initiated once the request becomes the EMIF's highest priority task, according to the priority scheme detailed in Section 13.2.13. In the event that the read request cannot be serviced by a single access cycle to the external device, multiple access cycles are performed by EMIF until the entire request is fulfilled. The details of an asynchronous read operation in normal mode are described in Table 13-21. Also, Figure 13-11 shows an example timing diagram of a basic read operation.
| Time Interval | Pin Activity in Normal Mode | |
|---|---|---|
| Turnaround period | Once the read operation becomes the highest priority task for EMIF, the EMIF waits for the programmed number of turn-around cycles before proceeding to the setup period of the operation. The number of wait cycles is taken directly from the TA field of the asynchronous n configuration register (ASYNC_CSn_CR). Between each access (write or read), the EMIF inserts two cycles of delay even though TA field is programmed as 0. After the EMIF has waited for the turnaround cycles to complete, the EMIF again checks to make sure that the read operation is still the highest priority task. If so, the EMIF proceeds to the setup period of the operation. If the read operation is no longer the highest priority task, the EMIF terminates the operation. | |
| Start of the setup period | The following actions occur at the start of the setup period:
| |
| Strobe period | The following actions occur during the strobe period of a read operation:
| |
| End of the hold period | At the end of the hold period:
| |
Figure 13-11 Timing Waveform of an Asynchronous Read Cycle in Normal Mode