SLUUCN4A January 2023 – February 2024
The BQ40Z50-R5 device can shut down upon the assertion of the DISP pin when the configuration bits [IO_SHUT] = 1 and [LED_EN] = 0. This feature is disabled when the LED display is enabled. When the pin is asserted for IO Shutdown Delay, the gas gauge opens its DSG FET, then shuts down once PACK voltage < Charger Present Threshold. If the pin is deasserted or [IO_TIMEOUT] is set and IO Shutdown Timeout expires following activation before PACK voltage < Charger Present Threshold, then the shutdown is stopped and the DSG FET turns back on and returns to the state it was in before the pin was asserted. An active low signal is detected when [IO_POL] = 0. An active high signal is detected when [IO_POL] = 1. An internal pullup is enabled when [IO_PUL_DIS] = 0. The pullup is disabled when [IO_PUL_DIS] = 1. The pin is sampled every 250 ms.
Status | Condition | Action |
---|---|---|
Trip | DISP asserted AND the [IO_SHUT] bit is set. | Turn DSG FET off |
Shutdown | Voltage at PACK pin < Charger Present Threshold | Send device into SHUTDOWN mode. |
Exit | Voltage at PACK pin > VSTARTUP | OperationStatus()[IOSHUT] = 0 Return to NORMAL mode. |