SLUUCN4A January 2023 – February 2024
The BQ40Z50-R5 SMBus address (default 0x16) can be changed. The target address should be programmed in Address and the 2’s complement of that value should be programmed in Address Check.
The BQ40Z50-R5 will check these values upon exit from POR, and if the two data flash values are not valid or the programmed address is 0x00 or 0xFF, then the device defaults to 0x16.
Class | Subclass | Name | Format | Size in Bytes | Min Value | Max Value | Default Value | Unit |
---|---|---|---|---|---|---|---|---|
Settings | SMBus | Address | Hex | 1 | 0x00 | 0xFF | 0x16 | — |
Class | Subclass | Name | Format | Size in Bytes | Min Value | Max Value | Default Value | Unit |
---|---|---|---|---|---|---|---|---|
Settings | SMBus | Address Check | Hex | 1 | 0x00 | 0xFF | 0xEA | — |
For details on SMBus specifications, visit http://www.smbus.org/specs/.