SLUUCN4A January 2023 – February 2024
As a part of the Impedance Track algorithm, the BQ40Z50-R5 calculates an RScale value. The RScale value can be applied in two ways:
This can prevent early termination of certain simulations, as the RScale will not be applied in computing voltages at DODs below RScale DOD. As a result, sensitivity to passed charge error is drastically decreased for low resistance and high resistance cells.