SLUUCN4A January 2023 – February 2024
This command enables/disables control of the CHG, DSG, and PCHG FETs by the firmware. The initial setting is loaded from Mfg Status Init[FET_EN]. If the ManufacturingStatus()[FET_EN] = 0, sending this command allows the FW to control the PCHG, CHG, and DSG FETs and the ManufacturingStatus()[FET_EN] = 1 and vice versa.
In UNSEALED mode, the ManufacturingStatus()[FET_EN] status is copied to Mfg Status Init[FET_EN] when the command is received by the gauge. The BQ40Z50-R5 device remains on its latest FET control status prior to a reset.