SLUUCN4A January 2023 – February 2024
Class | Subclass | Name | Type | Min | Max | Default | Unit |
---|---|---|---|---|---|---|---|
Calibration | Interconnect Resistance | Cell 3 | I2 | 0 | 1000 | 0 | mΩ |
Description: This is the interconnect resistance value entered by the user that represents the interconnect resistance between the top of Cell 2 and the bottom of the Cell 3, plus the interconnect resistance of the connection from the bottom of Cell 3 to the gauge. The measured CellVoltage3() is compensated for the voltage drop introduced by this resistance.