SLUUCN4A January 2023 – February 2024
This command enables/disables Lifetime Data Collection to help streamline production testing. The initial setting is loaded from Mfg Status Init[LF_EN]. If the ManufacturingStatus()[LF_EN] = 0, sending this command starts the Lifetime Data Collection and the ManufacturingStatus()[LF_EN] = 1 and vice versa.
In UNSEALED mode, the ManufacturingStatus()[LF_EN] status is copied to Mfg Status Init[LF_EN] when the command is received by the gauge. The BQ40Z50-R5 device remains on its latest Lifetime Data Collection setting prior to a reset.