SPRUJC6B October 2025 – April 2026 AM2752-Q1 , AM2754-Q1
Reset isolation is provided by LPSCs, and the feature is turned off by default. If an IP needs to be reset isolated, then SMS needs to enable this feature through the MMR configurations of that LPSC. If that LPSC supports multiple IPs, then all those IPs will be reset isolated. LPSC settings go back to default srata when the device goes through a power on reset. If reset isolation is not enabled, the LPSC returns back to the default start during warm resets.