SPRUJC6B October 2025 – April 2026 AM2752-Q1 , AM2754-Q1
The counter-compare submodule is responsible for generating two independent compare events based on two compare registers:
For up-count or down-count mode, each event occurs only once per cycle. For up-down-count mode each event occurs twice per cycle, if the compare value is between 0000h and TBPRD; and occurs once per cycle, if the compare value is equal to 0000h or equal to TBPRD. These events are fed into the action-qualifier submodule where they are qualified by the counter direction and converted into actions if enabled. Refer to Section 12.5.3.4.4 for more details.
The counter-compare EPWM_CMPA and EPWM_CMPB registers each have an associated shadow register. Shadowing provides a way to keep updates to the registers synchronized with the hardware. When shadowing is used, updates to the active registers only occurs at strategic points. This prevents corruption or spurious operation due to the register being asynchronously modified by software. The memory address of the active register and the shadow register is identical. Which register is written to or read from is determined by the EPWM_CMPCTL[4] SHDWAMODE and EPWM_CMPCTL[6] SHDWBMODE bits. These bits enable and disable the EPWM_CMPA shadow register and EPWM_CMPB shadow register respectively. The behavior of the two load modes is described below:
If the shadow register is enabled then the content of the shadow register is transferred to the active register on one of the following events:
Which of these three events will drive the counter compare module is specified by the EPWM_CMPCTL[1-0] LOADAMODE and EPWM_CMPCTL[3-2] LOADBMODE register bit fields. Only the active register contents are used by the counter-compare submodule to generate events to be sent to the action-qualifier.
Figure 12-311 and Figure 12-312 show Compare A and B Dual Shadow registers.
Figure 12-311 Compare A Dual Shadow register
Figure 12-312 Compare B Dual Shadow register