SPRUJC6B October 2025 – April 2026 AM2752-Q1 , AM2754-Q1
Events mapped to the high priority error interrupt are intended to be events that require immediate intervention from the system because a potentially dangerous error has occurred. An example would be an event indicating an uncorrected error. The system will want to diagnose the issue and intervene to ensure there are no violations.
Any error event can be mapped to the high priority error interrupt. A high priority error interrupt will be generated when an event is enabled to cause an interrupt (via the ESM_INTR_EN_SET_j) register and mapped to the high priority interrupt (via the ESM_INT_PRIO_j) register and the raw status is set (via the ESM_RAW_j).
When a high priority error interrupt is received, the acting processor must perform the following steps:
The global event map is neither defined by nor maintain in ESM. The global event map must be defined and maintained by software using software determined memory resources. It is conceivable that the global event map will be predefined and loaded during the execution of a secondary boot loader.
The rest of the steps assume that the error has been handled and the system wants to clear the error event. Clearing the error event depends on whether the event is a level (see Section 12.7.2.4.1.3.1) or pulse (see Section 12.7.2.4.1.3.2) event.