SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
In addition to the pipeline there are a few other behaviors of the DMA that affect the total throughput:
For example, to transfer 128 16-bit words from GS0 RAM to GS3 RAM, a channel can be configured to transfer 8 bursts of 16 words/burst. This gives:
| 8 bursts ˟ [(3 cycles/word ˟ 16 words/burst) + 1] = 392 cycles |
If instead the channel were configured to transfer the same amount of data 32 bits at a time (the word size is configured to 32 bits), the transfer can take:
| 8 bursts ˟ [(3 cycles/word ˟ 8 words/burst) + 1] = 200 cycles |
The DMA module consists of a 3-stage pipeline as shown in Figure 11-5 and Figure 11-6.
Figure 11-5 3-Stage Pipeline DMA Transfer
Figure 11-6 3-stage Pipeline with One Read Stall