SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
In idle-line multiprocessor mode, a frame that is preceded by an idle period (10 or more idle bits) is an address frame. A frame that is preceded by fewer than 10 idle bits is a data frame. Figure 28-6 illustrates the format of several blocks and frames with idle-line mode.
There are two ways to transmit an address frame using idle-line mode:
Method 1: In software, deliberately leave an idle period between the transmission of the last data frame of the previous block and the address frame of the new block.
Method 2: Configure the SCI to automatically send an idle period between the last data frame of the previous block and the address frame of the new block.
Although Method 1 is only accomplished by a delay loop in software, Method 2 can be implemented by using the transmit buffer and the TXWAKE bit in the following manner:
Step 1: Write a 1 to the TXWAKE bit.
Step 2: Write a dummy data value to the SCITD register. This triggers the SCI to begin the idle period as soon as the transmitter shift register is empty.
Step 3: Wait for the SCI to clear the TXWAKE flag.
Step 4: Write the address value to SCITD.
As indicated by Step 3, software can wait for the SCI to clear the TXWAKE bit. However, the SCI clears the TXWAKE bit at the same time the SCI sets TXRDY (that is, transfers data from SCITD into SCITXSHF). Therefore, if the TX INT ENA bit is set, the transfer of data from SCITD to SCITXSHF causes an interrupt to be generated at the same time that the SCI clears the TXWAKE bit. If this interrupt method is used, software is not required to poll the TXWAKE bit waiting for the SCI to clear the bit.
When idle-line multiprocessor communications are used, software must make sure that the idle time exceeds 10 bit periods before addresses (using one of the methods mentioned above), and software must also make sure that data frames are written to the transmitter quickly enough to be sent without a delay of 10 bit periods between frames. Failure to comply with these conditions results in data interpretation errors by other devices receiving the transmission.
Figure 28-6 Idle-Line Multiprocessor
Communication Format