SPRUJF8 May 2026 TMS320F28P551SG
FILE: erad_ex6_interrupt_order.c
This example uses a COUNTER to monitor the sequence of ISRs executed. An interrupt is generated if the ISRs executed are not in the expected order. The expected order is CPUTimer0 ,then CPUTimer1 and then CPUTimer2
The counter is configured in Start-Stop Mode to count the number of times CPUTimer2 interrupt occurs between the CPUTimer0 interrupt and CPUTimer1 ISRs. Ideally, this count should be zero if the interrupts are occurring in the expected order. we configure a threshold value of 1 to generate an RTOS interrupt. This indicates that the CPUTimer2 interrupt has come out of order.
For demonstration purposes, this example disables CPUTimer1 to simulate this error.
Watch Variables
External Connections