SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
The following are Flash module configuration settings at power-up:
During the boot process, the boot ROM performs a dummy read of the Code Security Module (CSM) password locations in the OTP. This read is performed to unlock a new device that has no password stored in the device, so that Flash programming or loading of code into CSM-protected SRAM can be performed. On devices with a password, this read has no effect and the device remains locked.
To achieve optimum system performance, user application software must initialize wait-states using the FRDCNTL register, and configure cache/prefetch features using the FRD_INTF_CTRL register. Software that configures Flash settings like wait-states, cache/prefetch features, and so on, must be executed only from RAM memory, not from Flash memory.