SPRUJF8 May 2026 TMS320F28P551SG
FILE: lpm_ex4_standbywake_watchdog.c
This example puts the device into STANDBY mode. If the lowest possible current consumption in STANDBY mode is desired, the JTAG connector must be removed from the device board while the device is in STANDBY mode.
This example puts the device into STANDBY mode then wakes up the device from STANDBY using watchdog timer.
The device wakes up from the STANDBY mode when the watchdog timer overflows triggering an interrupt. In the ISR, the GPIO1 is pulled low. the GPIO1 is toggled to indicate the device is out of STANDBY mode. A prescalar is set for the watchdog timer to change the counter overflow time.
GPIO1 is pulled high before entering the STANDBY mode and is pulled low when in the wakeup ISR.
External Connections