SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
eCAP modules can be synchronized with each other by selecting a common SYNCIN source. SYNCIN source for eCAP can be either software sync-in or external sync-in. The external sync-in signal can come from eCAP, X-Bar, or ePWM. The SWSYNC of the eCAP module is logical ORed with the SYNC signal as shown in Figure 19-7. The SYNC signal is defined by the selection of ECAPxSYNCINSEL[SEL] as shown in Figure 19-8.
Figure 19-7 ECAP Counter and Synchronization Block
Figure 19-8 eCAP Synchronization Scheme