SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
Figure 30-5 shows the CBC feedback mode of operation, where the input data is XORed with the IV before it is passed to the basic cryptographic core. The output of the cryptographic core passes directly to the output buffer and becomes the next IV.
The operation is reversed for decryption, resulting in an XOR at the output of the cryptographic core. The input cipher text of the current operation is the IV for the next operation.
Figure 30-6 AES - CBC Feedback Mode