SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
As long as each set of SOCs has identical trigger select and ACQPS settings, multiple trigger sources can be used while still achieving synchronous operation.
The following example demonstrates synchronous operation between ADCA and ADCC while using three SOCs and two trigger sources. Figure 14-31 demonstrates that any combination of relative trigger timings still results in synchronous operation.
Example: Synchronous Operation With Multiple Trigger Sources
AdcaRegs.ADCSOC0CTL.bit.CHSEL = 4; //SOC0 converts ADCINA4
AdcaRegs.ADCSOC0CTL.bit.ACQPS = 19; //SOC0 uses sample duration of 20 SYSCLK cycles
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 10; //SOC0 begins conversion on ePWM3 SOCB
AdccRegs.ADCSOC0CTL.bit.CHSEL = 0; //SOC0 converts ADCINC0
AdccRegs.ADCSOC0CTL.bit.ACQPS = 19; //SOC0 uses sample duration of 20 SYSCLK cycles
AdccRegs.ADCSOC0CTL.bit.TRIGSEL = 10; //SOC0 begins conversion on ePWM3 SOCB
AdcaRegs.ADCSOC1CTL.bit.CHSEL = 4; //SOC1 converts ADCINA4
AdcaRegs.ADCSOC1CTL.bit.ACQPS = 30; //SOC1 uses sample duration of 31 SYSCLK cycles
AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 10; //SOC1 begins conversion on ePWM3 SOCB
AdccRegs.ADCSOC1CTL.bit.CHSEL = 1; //SOC1 converts ADCINC1
AdccRegs.ADCSOC1CTL.bit.ACQPS = 30; //SOC1 uses sample duration of 31 SYSCLK cycles
AdccRegs.ADCSOC1CTL.bit.TRIGSEL = 10; //SOC1 begins conversion on ePWM3 SOCB
AdcaRegs.ADCSOC2CTL.bit.CHSEL = 0; //SOC2 converts ADCINA0
AdcaRegs.ADCSOC2CTL.bit.ACQPS = 19; //SOC2 uses sample duration of 20 SYSCLK cycles
AdcaRegs.ADCSOC2CTL.bit.TRIGSEL = 2; //SOC2 begins conversion on CPU Timer1
AdccRegs.ADCSOC2CTL.bit.CHSEL = 2; //SOC2 converts ADCINC2
AdccRegs.ADCSOC2CTL.bit.ACQPS = 19; //SOC2 uses sample duration of 20 SYSCLK cycles
AdccRegs.ADCSOC2CTL.bit.TRIGSEL = 2; //SOC2 begins conversion on CPU Timer1
Figure 14-31 Example: Synchronous Operation
with Multiple Trigger SourcesNote that any trigger source that can be selected in the TRIGSEL field can be used except for software triggering. There is no way to issue the software triggers for all ADCs simultaneously, so this results in asynchronous operation. ADCINT1 or ADCINT2 can also be used as a trigger when the ADCINTSOCSEL1 and ADCINTSOCSEL2 registers are configured identically for all ADCs and software triggering is not used to start the chain of conversions.