SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
Table 6-3 lists the memory-mapped registers for the FLASH_CTRL_REGS registers. All register offset addresses not listed in Table 6-3 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | FRDCNTL | Flash Read Control Register | EALLOW | Go |
| 4h | FLPROT | Flash program/erase protect register | EALLOW | Go |
| 180h | FRD_INTF_CTRL | Flash Read Interface Control Register | EALLOW | Go |
Complex bit access types are encoded to fit into small table cells. Table 6-4 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
FRDCNTL is shown in Figure 6-5 and described in Table 6-5.
Return to the Summary Table.
Flash Read Control Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | RESERVED | ||||||
| R-0h | R/W-Fh | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | RWAIT | ||||||
| R-0h | R/W-Fh | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-28 | RESERVED | R | 0h | Reserved |
| 27-24 | RESERVED | R/W | Fh | Reserved |
| 23-12 | RESERVED | R | 0h | Reserved |
| 11-8 | RWAIT | R/W | Fh | Random read waitstate These bits indicate how many waitstates are added to a flash read/fetch access. The RWAIT value can be set anywhere from 0 to 0xF. For a flash access, data is returned in RWAIT+1 SYSCLK cycles. Note: The required wait states for each SYSCLK frequency can be found in the device data manual. Reset type: SYSRSn |
| 7-0 | RESERVED | R | 0h | Reserved |
FLPROT is shown in Figure 6-6 and described in Table 6-6.
Return to the Summary Table.
Flash program/erase protect register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | FLWEPROT | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | FLWEPROT | R/W | 0h | Flash program/erase protect bit. 0 : Program erase operation allowed subject to security settings. 1 : Program erase operation blocked in hardware. Reset type: SYSRSn |
FRD_INTF_CTRL is shown in Figure 6-7 and described in Table 6-7.
Return to the Summary Table.
Flash Read Interface Control Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | DATA_CACHE_EN | PREFETCH_EN | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-2 | RESERVED | R | 0h | Reserved |
| 1 | DATA_CACHE_EN | R/W | 0h | Data cache enable. 0 A value of 0 disables the data cache. 1 A value of 1 enables the data cache. Reset type: SYSRSn |
| 0 | PREFETCH_EN | R/W | 0h | Prefetch enable. 0 A value of 0 disables prefetch mechanism. 1 A value of 1 enables pre-fetch mechanism. Reset type: SYSRSn |