SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
The CLB X-BAR brings signals to the CLB modules. Figure 10-3 shows the architecture of the CLB X-BAR. Note that the architecture of the CLB X-BAR is identical to the architecture of the GPIO Output X-BAR (with the exception of the output latch).