SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Secure Flash boot mode is similar to Flash boot mode in that the boot flow branches to the configured memory address in Flash except only after the Flash memory contents have been authenticated. The Flash authentication uses a Cipher-based Message Authentication Protocol (CMAC) to authenticate 16KB of Flash starting from the configured Flash entry point address. The CMAC calculation requires a user-defined 128-bit key programmed in the CPU User OTP Zone 1 Header OTP CMACKEY bit field. Additionally, calculate the golden CMAC tag based on the 16KB Flash memory range and store the CMAC tag along with the user code at a hardcoded address in Flash. During secure Flash boot, the calculated CMAC tag is compared to the user golden CMAC tag in Flash to determine the pass/fail status of the CMAC authentication. When authentication passes, boot flow continues and branches to Flash to begin executing the application. When authentication fails, the device is reset.
For the available secure Flash boot entry address options, refer to Section 4.7.2.
For generating the secure Flash golden CMAC tag for CPU, refer to the TMS320C28x Assembly Language Tools User’s Guide within section “Using Secure Flash Boot on TMS320F2838x Devices” for instructions.
Key: 2B7E1516 28AED2A6 ABF71588 09CF4F3C
(MSB is 2B and LSB is 3C)
CMACKEY0 = 0x2B7E1516
CMACKEY1 = 0x28AED2A6
CMACKEY2 = 0xABF71588
CMACKEY3 = 0x09CF4F3C
Make sure that the Flash sector that encompasses the configured Flash entry point and the first 16 KB of Flash is assigned to Zone 1 for the core setup for secure Flash boot.
Recommended to use device JTAGLOCK when using secure Flash boot.
APIs for CMAC calculation and authentication is provided as part of ROM. Details are available in Section 4.7.10
Name | Address | Details |
---|---|---|
CMAC Golden Tag (128-bit) |
CPU: Flash Entry Point Address + 0x2 |
Located in Flash, offset
from the entry point address, by 2 words (CPU). When CMAC calculations are performed, the golden tag location in memory is considered all 0xF. Refer to Example4-1 for an example regarding linker configuration on CPU. Lower memory contains the tag most-significant word (MSW) and higher memory contains the least-significant word (LSW). |
Example (on CPU): Tag = 0x0011 2233 4455 6677 8899 AABB CCDD EEFF Address 0x0 = 0x0011 2233 Address 0x2 = 0x4455 6677 Address 0x4 = 0x8899 AABB Address 0x6 = 0xCCDD EEFF |
||
CMAC 128-Bit Key | 0x0007 8018 | Located in CPU Zone 1 User
Header OTP (CMACKEY0, CMACKEY1, CMACKEY2, CMACKEY3) CMACKEY0 contains the key MSW and CMACKEY3 contains the LSW. |
Example: Key = 0x0011 2233 4455 6677 8899 AABB CCDD EEFF CMACKEY0 = 0x0011 2233 CMACKEY1 = 0x4455 6677 CMACKEY2 = 0x8899 AABB CMACKEY3 = 0xCCDD EEFF |
||
Address Range for CMAC Calculation | Start: Flash Entry Point Address End: Flash Entry Point Address + 16KB |
Option | BOOTDEFx Value | Flash Sector | Address | Devices Supported |
---|---|---|---|---|
0 | 0x0A | Bank 0 Sector 0 | 0x0008 0000 | All |
1 | 0x2A | Bank 0 Sector 32 | 0x0008 8000 | All |
2 | 0x4A | Bank 2 Sector 0 | 0x000C 0000 | All |
3 | 0x6A | Bank 2 Sector 32 | 0x000C 8000 | All |
4 | 0x83 | Bank 4 Sector 0 | 0x0010 0000 | Device Dependent |
CPU | Action on Failed Authentication |
---|---|
C28x CPU |
1. Emulation only - Halt debugger (ESTOP) 2. Wait in endless loop (for device reset due to a watchdog reset) |
Step | Action |
---|---|
1 | Secure Flash boot CPU |
2 | Any Flash beyond the first 16KB from the entry point that is planned for use can be authenticated by the user using a different CMAC golden tag embedded at an address somewhere within the already authenticated 16KB of Flash. |