SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
For a shared RAM, multiple accesses can happen at any given time. The maximum number of accesses to any shared RAM at any given time depends on the type of shared RAM. On this device, a combination of a fixed and alternating scheme is followed to arbitrate multiple access at any given time.
The following is the order of fixed priority for CPU accesses:
The following is the order of fixed priority for CLA accesses:
Figure 3-16 represents the arbitration scheme on local shared memories.
Figure 3-17 represents the arbitration scheme on global shared memories