SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The RX_TRIGx external trigger can be used to initiate FSITX transmission. RX_TRIG0 must be used if TDM mode (multi-node configuration) is required. RX_TRIG0 must be used as the trigger source for start of transmission while the programmable stretch width RX_TRIG0 signal is used as the SEL_TDM_PATH signal (which decides whether the local FSITX is active or put in bypass mode).
The signal source for the RX_TRIGx signal is selected through the RX_TRIG_CTRL_x.TRIG_SEL bits, as listed in Table 24-11.
RX_TRIG_CTRLx.TRIG_SEL | Selected Signal |
---|---|
0 | Ping Packet Received |
1 | Data Packet Received |
2 | Error Packet Received |
3 | Ping Frame Tag Match Occurred |
4 | Data Frame Tag Match Occurred |
5 | Error Frame Tag Match Occurred |
6 | Frame Done |
7 | Reserved |
8 to 15 | Reserved |
The RX_TRIGx signals can optionally be delayed (this can be used in TDM scenarios) through the RX_TRIG_CTRL_x.TRIG_DLY.