SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Load the 32-Bits of a 32-Bit Floating-Point Register
This instruction is an alias for the MMOVIZ and MMOVXI instructions. The second operand is translated by the assembler such that the instruction becomes:
MMOVIZ MRa, #16FHiHex MMOVXI MRa, #16FLoHex
MRa | CLA floating-point destination register (MR0 to MR3) |
#32F | Immediate float value represented in floating-point representation |
LSW: IIII IIII IIII IIII (opcode of MMOVIZ MRa, #16FHiHex)
MSW: 0111 1000 0100 00aa
LSW: IIII IIII IIII IIII (opcode of MMOVXI MRa, #16FLoHex)
MSW: 0111 1000 1000 00aa
This instruction accepts the immediate operand only in floating-point representation. To specify the immediate value as a hex value (IEEE 32-bit floating- point format), use the MOVI32 MRa, #32FHex instruction.
Load the 32-bits of MRa with the immediate float value represented by #32F.
#32F is a float value represented in floating-point representation. The assembler only accepts a float value represented in floating-point representation. That is, 3.0 can only be represented as #3.0 (#0x40400000 results in an error).
MRa = #32F;
This instruction modifies the following flags in the MSTF register:
Flag | TF | ZF | NF | LUF | LVF |
---|---|---|---|---|---|
Modified | No | No | No | No | No |
Depending on #32F, this instruction takes one or two cycles. If all of the lower 16-bits of the IEEE 32-bit floating-point format of #32F are zeros, then the assembler converts MMOVF32 into only an MMOVIZ instruction. If the lower 16-bits of the IEEE 32-bit floating-point format of #32F are not zeros, then the assembler converts MMOVF32 into MMOVIZ and MMOVXI instructions.
MMOVF32 MR1, #3.0 ; MR1 = 3.0 (0x40400000)
; Assembler converts this instruction as
; MMOVIZ MR1, #0x4040
MMOVF32 MR2, #0.0 ; MR2 = 0.0 (0x00000000)
; Assembler converts this instruction as
; MMOVIZ MR2, #0x0
MMOVF32 MR3, #12.265 ; MR3 = 12.625 (0x41443D71)
; Assembler converts this instruction as
; MMOVIZ MR3, #0x4144
; MMOVXI MR3, #0x3D71