SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The receiver tag registers (receiver frame tag and user data (RX_FRAME_TAG_UDATA) register and receiver ping tag (RX_PING_TAG) register)) have the least-significant bit set to 0. The actual received tag is in the bit positions 4:1. The reason for this is to facilitate user software to create a table of functions that can be called depending on the tag value. A function pointer needs a 32-bit storage space and, hence, each successive pointer is offset by 2. If the first pointer is at address x, then the second pointer is at address x + 2, the third at address x + 4, and so on. By keeping the LSB to 0, the five bits of the tag register (bits 4:0) can now be directly used as an index into a table of function pointers.