SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The SEC units count accurately only when the CPU is operating in normal conditions. If the counters are running and capturing the CPU cycles while the CPU is controlled through the debugger to single-step through the code, then the result can differ from when the CPU was executing the code in normal conditions.
Note that if the counters are set up to use the value of the raw program counter register (VPC) as the source for the start and stop events, the value of the CPU cycles measured can be off by a few cycles when the CALL instruction is executed.