SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
This section includes information on the available interrupts present in the SPI module. The SPI module contains two interrupt lines: SPIINT/SPIRXINT and SPITXINT. When the SPI is operating in non-FIFO mode, all available interrupts are routed together to generate the single SPIINT interrupt. When FIFO mode is used, both SPIRXINT and SPITXINT can be generated.
SPIINT/SPIRXINT
When the SPI is operating in non-FIFO mode, the interrupt generated is called SPIINT. If FIFO enhancements are enabled, the interrupt is called SPIRXINT. These interrupts share the same interrupt vector in the Peripheral Interrupt Expansion (PIE) block.
In non-FIFO mode, two conditions can trigger an interrupt: a transmission is complete (INT_FLAG), or there is overrun in the receiver (OVERRUN_FLAG). Both of these conditions share the same interrupt vector: SPIINT.
The transmission complete flag (INT_FLAG) indicates that the SPI has completed sending or receiving the last bit and is ready to be serviced. At the same time this bit is set, the received character is placed in the receiver buffer (SPIRXBUF). The INT_FLAG generates an interrupt on the SPIINT vector if the SPIINTENA bit is set.
The receiver overrun flag (OVERRUN_FLAG) indicates that a transmit or receive operation has completed before the previous character has been read from the buffer. The OVERRUN_FLAG generates an interrupt on the SPIINT vector if the OVERRUNINTENA bit is set and OVERRUN_FLAG was previously cleared.
In FIFO mode, the SPI can interrupt the CPU upon a match condition between the current receive FIFO status (RXFFST) and the receive FIFO interrupt level (RXFFIL). If RXFFST is greater than or equal to RXFFIL, the receive FIFO interrupt flag (RXFFINT) is set. SPIRXINT is triggered in the PIE block, if RXFFINT is set and the receive FIFO interrupt is enabled (RXFFIENA = 1).
SPITXINT
The SPITXINT interrupt is not available when the SPI is operating in non-FIFO mode.
In FIFO mode, the SPITXINT behavior is similar to the SPIRXINT. SPITXINT is generated upon a match condition between the current transmit FIFO status (TXFFST) and the transmit FIFO interrupt level (TXFFIL). If TXFFST is less than or equal to TXFFIL, the transmit FIFO interrupt flag (TXFFINT) is set. SPITXINT is triggered in the PIE block, if TXFFINT is set and the transmit FIFO interrupt is enabled in the SPI module (TXFFIENA = 1).
Figure 21-2 and Table 21-2 show how these control bits influence the SPI interrupt generation.
FIFO Options | SPI Interrupt Source | Interrupt Flags | Interrupt Enables | FIFO Enable (SPIFFENA) | Interrupt Line (1) |
---|---|---|---|---|---|
SPI without FIFO | Receive overrun | RXOVRN | OVRNINTENA | 0 | SPIRXINT |
Data receive | SPIINT | SPIINTENA | 0 | SPIRXINT | |
Transmit empty | SPIINT | SPIINTENA | 0 | SPIRXINT | |
SPI FIFO mode | FIFO receive | RXFFIL | RXFFIENA | 1 | SPIRXINT |
Transmit empty | TXFFIL | TXFFIENA | 1 | SPITXINT |