SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
In certain systems where the ADC successively samples multiple signal sources, memory crosstalk can occur. Memory crosstalk is the tendency of the ADC conversion to be pulled towards the value of the previous conversion, due to inadequate acquisition/settling time. This happens because the ADC sample capacitor voltage starts near the previously converted voltage, then settles towards the newly applied voltage on the current channel. If the acquisition window is not long enough for the sample capacitor to settle, this can result in some sample error reflected in the ADC conversion.
The 12-bit ADC modules in this device include a sample capacitor reset feature to help mitigate memory crosstalk. When sample capacitor reset is enabled, after every conversion, the sampling capacitor voltage is reset to the VREFLO voltage. This reset takes an extra ADCCLK cycle to complete. The sample capacitor reset function is inactive by default for each SOC. If desired, the application can activate sample capacitor reset by writing 0 to the SAMPCAPRESET bit in the ADCSOCxCTL register. When sample capacitor reset is active, overall ADC throughput is slightly decreased due to the extra ADCCLK cycle in the conversion period.