- Launch Code Composer Studio v5.5: Start > All Programs > Texas Instruments > Code Composer Studio 5.5.0 > Code Composer Studio 5.5.0
- Create new Workspace or open existing Workspace that does not yet contain eZ430-Chronos projects
NOTE
Workspaces should not be located in a long path of directories as Windows only supports path names up to 255 characters. Keep in mind that the projects contain subdirectories as well.
- Import eZ430-Chronos Projects by clicking: Project > Import Existing CCS Eclipse Project
- Click Browse and browse to eZ430-Chronos Projects (C:\Program Files\Texas Instruments\eZ430-Chronos\Software Projects\Chronos Watch\CCS ). Confirm directory by clicking OK
- The eZ430-Chronos demo project appears as ez430_chronos, the eZ430-Chronos data logger appears as ez430_chronos_datalogger. Check the boxes Copy projects into workspace and Automatically import referenced projects to create a new copy of the projects
- Click Finish to finalize the project import. The projects appear in the C/C++ Projects view of CCS
- Select the right version of the project. Each project comes with six different project settings (build configurations), which can be selected in Project > Properties > C/C++ Build > Active Configuration > Configuration:
915 MHz – Limited CCS Core Edition (USA)
868 MHz – Limited CCS Core Edition (Europe)
433 MHz – Limited CCS Core Edition (Other regions)
915 MHz – Unrestricted CCS Platinum (USA)
868 MHz – Unrestricted CCS Platinum (Europe)
433 MHz – Unrestricted CCS Platinum (Other regions)
- Go to Run > Debug to launch the debugger