SLAU292G November 2009 – July 2015
Press * until the temperature mode is active (see Figure 3-1 for details). The temperature can be shown in degree Celsius or Fahrenheit. The selection depends on the time mode setting. In 12H mode, the temperature is shown in degrees Fahrenheit, in 24H mode in degrees Celsius. The temperature is measured in 1-second intervals. Positive temperatures are marked with a small arrow pointing up in the upper LCD line, left of the temperature. An arrow pointing down indicated temperatures below zero.
Secondary function: None
Set function: Temperature calibration (can also calibrated from PC software in Sync mode, see Section 3.3).
NOTE
The temperature is measured inside the wrist module by the CC430 device. When the wrist module is worn, its temperature may be different from the surrounding temperature due to body heat. For accurate temperature measurements, do not wear the wrist module and allow a sufficient amount of time for the wrist module to adapt to the surrounding temperature.